Solid Edge FrameworkSupport Type Library
SegmentedStyleCount Property
Description
Returns the number of segmented styles defined for the referenced graphic object.
Property type
Read-only property
Syntax
Visual Basic
Public Property SegmentedStyleCount As Long
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFrameWork.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objSheet As SolidEdgeDraft.Sheet
    Dim objEllpArc As SolidEdgeFrameworkSupport.EllipticalArc2d
    Dim objLinStyle As SolidEdgeFrameWork.LinearStyle
    Dim dblStrt As Double
    Dim dblFin As Double
    Dim strStyleName As String, strStyleParent As String
    Dim xStart As Double, yStart As Double, xEnd As Double, yEnd As Double
    Dim lngCnt As Long
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
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'getting the Active Sheet object
    Set objSheet = objDoc.ActiveSheet
    'Create an EllipticalArc object
    dblStrt = 180 * PI / 180
    dblFin = 230 * PI / 180
    Set objEllpArc = objSheet.EllipticalArcs2d.AddByCenter(xCenter:=0.25, yCenter:=0.25, _
                                                           xMajoraxis:=0.03, yMajoraxis:=0.02, Ratio:=0.5, _
                                                           Orientation:=0, StartAngle:=dblStrt, EndAngle:=dblFin)

    ' Create a LinearStyle2d Object
    strStyleName = "LinearStyleDotted"
    strStyleParent = "Dotted"
    Set objLinStyle = objDoc.LinearStyles.Add(Name:=strStyleName, Parent:=strStyleParent)
    ' Get the Start point of the EllipticalArc
    Call objEllpArc.GetStartPoint(x:=xStart, y:=yStart)
    ' Get the End point of the EllipticalArc
    Call objEllpArc.GetEndPoint(x:=xEnd, y:=yEnd)
    Call objEllpArc.AddSegmentedStyle(x1:=xStart + 0.05, y1:=yStart + 0.05, x2:=xEnd + 0.05, y2:=yEnd + 0.05, Style:=objLinStyle)
    ' Get the SegmentedStyle Count on the EllipticalArc object
    lngCnt = objEllpArc.SegmentedStyleCount
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSheet = Nothing
    Set objEllpArc = Nothing
    Set objLinStyle = Nothing
End Sub
See Also

EllipticalArc2d Object  | EllipticalArc2d Members