Solid Edge FrameworkSupport Type Library
SendBackward Method
Description
Changes the display order of visible objects by moving the referenced object so that it is in back of the first object behind it.
Syntax
Visual Basic
Public Sub SendBackward() 
Remarks
This command is useful when objects are hiding other objects that have a lower priority display but when you do not want to send the object all the way to the back of the priority list.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFrameWork.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objSheet As SolidEdgeDraft.Sheet
    Dim objEllpArc As SolidEdgeFrameworkSupport.EllipticalArc2d
    Dim objCircle As SolidEdgeFrameworkSupport.Circle2d
    Dim objLine As SolidEdgeFrameworkSupport.Line2d
    Dim dblStrt As Double
    Dim dblFin As Double
    Dim lngZOrder1 As Long
    Dim lngZOrder2 As Long
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
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'getting the Active Sheet object
    Set objSheet = objDoc.ActiveSheet
    ' Create Line and Circle object intersecting the EllipticalArc
    Set objLine = objSheet.Lines2d.AddBy2Points(x1:=0.1, y1:=0.1, x2:=0.5, y2:=0.2)
    Set objCircle = objSheet.Circles2d.AddByCenterRadius(x:=0.2, y:=0.2, Radius:=0.1)
    'Create an EllipticalArc object
    dblStrt = 180 * PI / 180
    dblFin = 230 * PI / 180
    Set objEllpArc = objSheet.EllipticalArcs2d.AddByCenter(xCenter:=0.25, yCenter:=0.25, _
                                                           xMajoraxis:=0.03, yMajoraxis:=0.02, Ratio:=0.5, _
                                                           Orientation:=0, StartAngle:=dblStrt, EndAngle:=dblFin)
    lngZOrder1 = objEllpArc.ZOrder
    ' Send Backward the EllipticalArc object
    Call objEllpArc.SendBackward
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSheet = Nothing
    Set objEllpArc = Nothing
    Set objCircle = Nothing
    Set objLine = Nothing
End Sub
See Also

EllipticalArc2d Object  | EllipticalArc2d Members