Solid Edge FrameworkSupport Type Library
SetStartPoint Method
Specifies the new coordinates of the start point.
Specifies the new coordinates of the start point.
Description
Relocates the starting point of the referenced object.
Syntax
Visual Basic
Public Sub SetStartPoint( _
   ByVal x As Double, _
   ByVal y As Double _
) 
Parameters
x
Specifies the new coordinates of the start point.
y
Specifies the new coordinates of the start point.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objEllpArcs As SolidEdgeFrameworkSupport.EllipticalArcs2d
    Dim objEllpArc As SolidEdgeFrameworkSupport.EllipticalArc2d
    Dim dblStrt As Double
    Dim dblFin As Double
    Dim x As Double, y As Double
    Dim sDumpStatus As String    ' Used for temporary storage of datadump return string
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'Create an EllipticalArcs2d collection object
    Set objEllpArcs = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:= _
                                                          objDoc.RefPlanes(1)).EllipticalArcs2d
    'Create an EllipticalArc object
    dblStrt = 0 * 3.14159 / 180
    dblFin = 90 * 3.14159 / 180
    Set objEllpArc = objEllpArcs.AddByCenter(xCenter:=0, yCenter:=0, _
                                             xMajoraxis:=0.04, yMajoraxis:=0, Ratio:=0.5, _
                                             Orientation:=1, StartAngle:=dblStrt, EndAngle:=dblFin)
    If objEllpArcs.Count <> 1 Then
        MsgBox (" AddByCenter method of EllipticalArcs2d object failed")
    End If
    ' Set the Starting Point of the EllipticalArc
    Call objEllpArc.SetStartPoint(x:=0, y:=-0.02)
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objEllpArcs = Nothing
    Set objEllpArc = Nothing
End Sub
See Also

EllipticalArc2d Object  | EllipticalArc2d Members