Solid Edge FrameworkSupport Type Library
Type Property
Description
Specifies the type of the object being referenced.
Property type
Read-only property
Syntax
Visual Basic
Public Property Type As Long
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objEllpArcs As SolidEdgeFrameworkSupport.EllipticalArcs2d
    Dim objEllpArc As SolidEdgeFrameworkSupport.EllipticalArc2d
    Dim dblStrt As Double
    Dim dblFin As Double
    Dim cType As ObjectType
    Dim sDumpStatus As String    ' Used for temporary storage of datadump return string
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'Create an EllipticalArcs2d collection object
    Set objEllpArcs = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:= _
                                                          objDoc.RefPlanes(1)).EllipticalArcs2d
    'Create an EllipticalArc object
    dblStrt = PI
    dblFin = 230 * 3.14159 / 180
    Set objEllpArc = objEllpArcs.AddByCenter(xCenter:=0.02, yCenter:=0.02, _
                                             xMajoraxis:=0.03, yMajoraxis:=0.02, Ratio:=0.5, _
                                             Orientation:=0, StartAngle:=dblStrt, EndAngle:=dblFin)
    ' Get the Type Property
    cType = objEllpArc.Type
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objEllpArcs = Nothing
    Set objEllpArc = Nothing
End Sub
See Also

EllipticalArc2d Object  | EllipticalArc2d Members