Solid Edge FrameworkSupport Type Library
Item Method
Variant (input) index.
Description
The items in a collection.
Syntax
Visual Basic
Public Function Item( _
   ByVal Index As Variant _
) As EllipticalArc2d
Parameters
Index
Variant (input) index.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objEllpArcs As SolidEdgeFrameworkSupport.EllipticalArcs2d
    Dim objEllpArc1 As SolidEdgeFrameworkSupport.EllipticalArc2d
    Dim objEllpArc2 As SolidEdgeFrameworkSupport.EllipticalArc2d
    Dim dblStrt As Double
    Dim dblFin As Double
    Dim sDumpStatus As String    ' Used for temporary storage of datadump return string
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'Create an Elliptical Arcs2d collection object
    Set objEllpArcs = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:= _
                                                          objDoc.RefPlanes(1)).EllipticalArcs2d
    'Create an EllipticalArc object
    dblStrt = 180 * 3.14159 / 180
    dblFin = 230 * 3.14159 / 180
    Set objEllpArc1 = objEllpArcs.AddByCenter(xCenter:=0.02, yCenter:=0.02, _
                                              xMajoraxis:=0.03, yMajoraxis:=0.02, Ratio:=0.5, _
                                              Orientation:=0, StartAngle:=dblStrt, EndAngle:=dblFin)
    ' Assign the EllipticalArc object to a new object
    Set objEllpArc2 = objEllpArcs.Item(1)
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objEllpArcs = Nothing
    Set objEllpArc1 = Nothing
    Set objEllpArc2 = Nothing
End Sub
See Also

EllipticalArcs2d Collection  | EllipticalArcs2d Members