Solid Edge FrameworkSupport Type Library
Application Property
Description
Returns the active application object.
Property type
Read-only property
Syntax
Visual Basic
Public Property Application As Application
Example
Private Sub Form_Load()

    Dim objApp As SolidEdgeFramework.Application

    Dim objDoc As SolidEdgeDraft.DraftDocument

    Dim objSheet As SolidEdgeDraft.Sheet

    Dim objFCFs As SolidEdgeFrameworkSupport.FeatureControlFrames

    Dim objFCFApp As SolidEdgeFramework.Application

    ' Local variables to be declared here
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
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")

        objApp.Visible = True

    Else

        Set objDoc = objApp.ActiveDocument

    End If

    On Error GoTo 0

    'Get the Active Sheet object

    Set objSheet = objDoc.ActiveSheet

    'Get the FeatureControlFrames collection object

    Set objFCFs = objSheet.FeatureControlFrames

    'Get the Application object from the FCF collection

    Set objFCFApp = objFCFs.Application

    ' Release objects

    Set objApp = Nothing

    Set objDoc = Nothing

    Set objSheet = Nothing

    Set objFCFs = Nothing

    Set objFCFApp = Nothing

End Sub
See Also

FeatureControlFrames Collection  | FeatureControlFrames Members