Solid Edge FrameworkSupport Type Library
ClearDataSet Method
Description
Restores the property settings applied to existing annotation objects.
Syntax
Visual Basic
Public Sub ClearDataSet() 
Remarks
These settings remain until the DataSet property of the annotation collection object is modified.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objSheet As SolidEdgeDraft.Sheet
    Dim objFCFs As SolidEdgeFrameworkSupport.FeatureControlFrames
    Dim objFCFDataSet As SolidEdgeFrameworkSupport.FeatureControlFrameDataSet
    ' Local variables to be declared here
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
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    On Error GoTo 0
    'Get the Active Sheet object
    Set objSheet = objDoc.ActiveSheet
    'Get the FeatureControlFrames collection object
    Set objFCFs = objSheet.FeatureControlFrames
    'Create a FeatureControlFrameDataSet to assign the same to FCF collection
    Set objFCFDataSet = objDoc.FeatureControlFrameDataSets.Add(Name:="MyDataSet")
    'Assign the created FeatureControlFrameDataSet to the FeatureControlFrames collection object
    objFCFs.DataSet = objFCFDataSet
    'Clear the DataSet associated with the FeatureControlFrames collection object
    Call objFCFs.ClearDataSet
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSheet = Nothing
    Set objFCFs = Nothing
    Set objFCFDataSet = Nothing
End Sub
See Also

FeatureControlFrames Collection  | FeatureControlFrames Members