Solid Edge FrameworkSupport Type Library
ClearStyle Method
Description
Clears any previously set style object.
Syntax
Visual Basic
Public Sub ClearStyle() 
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objSheet As SolidEdgeDraft.Sheet
    Dim objFCFs As SolidEdgeFrameworkSupport.FeatureControlFrames
    ' Local variables to be declared here
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
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    On Error GoTo 0
    'Get the Active Sheet object
    Set objSheet = objDoc.ActiveSheet
    'Get the FeatureControlFrames collection object
    Set objFCFs = objSheet.FeatureControlFrames
    'Set a style to the FeatureControlFrames collection object
    objFCFs.Style = objDoc.DimensionStyles(1)
    'Cleare the Style associated with the FeatureControlFrames collection object
    Call objFCFs.ClearStyle
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSheet = Nothing
    Set objFCFs = Nothing
End Sub
See Also

FeatureControlFrames Collection  | FeatureControlFrames Members