Solid Edge FrameworkSupport Type Library
DataSet Property
Description
Sets and returns a previously saved set of property settings to apply to newly created annotation objects.
Property type
Read-write property
Syntax
Visual Basic
Public Property DataSet As FeatureControlFrameDataSet
Remarks
These settings include the roughness value text, the active surface finish symbol, and so forth. The dimension style and leader on-off settings are not part of the data set.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objSheet As SolidEdgeDraft.Sheet
    Dim objFCFs As SolidEdgeFrameworkSupport.FeatureControlFrames
    Dim objFCFDataSet As SolidEdgeFrameworkSupport.FeatureControlFrameDataSet
    Dim objFCFDataSet1 As SolidEdgeFrameworkSupport.FeatureControlFrameDataSet
    ' Local variables to be declared here
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
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    On Error GoTo 0
    'Get the Active Sheet object
    Set objSheet = objDoc.ActiveSheet
    'Get the FeatureControlFrames collection object
    Set objFCFs = objSheet.FeatureControlFrames
    'Create a FeatureControlFrameDataSet to assign the same to FCF collection
    Set objFCFDataSet = objDoc.FeatureControlFrameDataSets.Add(Name:="MyDataSet")
    'Assign the created FeatureControlFrameDataSet to the FeatureControlFrames collection object
    objFCFs.DataSet = objFCFDataSet
    'Retrieve the FCFDataSet associated with the FCF collection object
    Set objFCFDataSet1 = objFCFs.DataSet
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSheet = Nothing
    Set objFCFs = Nothing
    Set objFCFDataSet = Nothing
    Set objFCFDataSet1 = Nothing
End Sub
See Also

FeatureControlFrames Collection  | FeatureControlFrames Members