Solid Edge FrameworkSupport Type Library
Style Property
Description
For collection objects, Body objects, RefPlane objects, Sketch objects, CoordinateSystem objects, CommandBarButton objects, SmartFrame2d objects, View objects, and TextCharStyle objects, Style is read-write. For all other objects, Style is read-only.
Property type
Read-write property
Syntax
Visual Basic
Public Property Style As DimensionStyle
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objSheet As SolidEdgeDraft.Sheet
    Dim objFCFs As SolidEdgeFrameworkSupport.FeatureControlFrames
    Dim objDimStyle As SolidEdgeFrameworkSupport.DimensionStyle
    Dim objDimStyle1 As SolidEdgeFrameworkSupport.DimensionStyle
    ' Local variables to be declared here
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
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    On Error GoTo 0
    'Get the Active Sheet object
    Set objSheet = objDoc.ActiveSheet
    'Get the FeatureControlFrames collection object
    Set objFCFs = objSheet.FeatureControlFrames
    'Create a DimensionStyle object
    Set objDimStyle = objDoc.DimensionStyles(1)
    'Assign the created DimensionStyle to the FeatureControlFrames collection object
    objFCFs.Style = objDimStyle
    'Get the Dimension Style associated with FeatureControlFrames collection object
    Set objDimStyle1 = objFCFs.Style
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSheet = Nothing
    Set objFCFs = Nothing
    Set objDimStyle = Nothing
    Set objDimStyle1 = Nothing
End Sub
See Also

FeatureControlFrames Collection  | FeatureControlFrames Members