Solid Edge FrameworkSupport Type Library
GetConnectedObjects Method
Returns the first object to which the chamfer or fillet connects.
Returns the second object to which the chamfer or fillet connects.
Description
Returns both objects connected to the referenced fillet or chamfer.
Syntax
Visual Basic
Public Sub GetConnectedObjects( _
   ByRef Obj1 As Object, _
   ByRef Obj2 As Object _
) 
Parameters
Obj1
Returns the first object to which the chamfer or fillet connects.
Obj2
Returns the second object to which the chamfer or fillet connects.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objArcs As SolidEdgeFrameworkSupport.Arcs2d
    Dim objArc1 As SolidEdgeFrameworkSupport.Arc2d
    Dim objL1 As SolidEdgeFrameworkSupport.Line2d
    Dim objL2 As SolidEdgeFrameworkSupport.Line2d
    Dim objFill As SolidEdgeFrameworkSupport.FilletGeometry2d
    Dim Obj1 As SolidEdgeFrameworkSupport.Line2d
    Dim Obj2 As SolidEdgeFrameworkSupport.Line2d
    Dim sDumpStatus As String    ' Used for temporary storage of datadump return string
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    ' Create an Arcs collection object
    Set objArcs = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:=objDoc.RefPlanes(1)).Arcs2d
    ' Create two intersecting line objects
    Set objL1 = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:=objDoc.RefPlanes(1)). _
                Lines2d.AddBy2Points(x1:=0, y1:=0, x2:=0.1, y2:=0)
    Set objL2 = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:=objDoc.RefPlanes(1)). _
                Lines2d.AddBy2Points(x1:=0, y1:=0.1, x2:=0, y2:=0)
    ' Create an arc object
    Set objArc1 = objArcs.AddAsFillet(Obj1:=objL1, Obj2:=objL2, Radius:=0.05, _
                                      xDirection:=0.15, yDirection:=0.05)
    ' Get the Fillet Properties
    Set objFill = objArc1.Fillet
    ' Get the Connected Objects
    Call objFill.GetConnectedObjects(Obj1:=Obj1, Obj2:=Obj2)
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objArcs = Nothing
    Set objL1 = Nothing
    Set objL2 = Nothing
    Set objArc1 = Nothing
    Set objFill = Nothing
    Set Obj1 = Nothing
    Set Obj2 = Nothing
End Sub
See Also

FilletGeometry2d Object  | FilletGeometry2d Members