Solid Edge FrameworkSupport Type Library
AutoPhase Property
Description
If True, specifies that the negative dash gaps for the referenced style object are automatically extended based on the size of the edge.
Property type
Read-write property
Syntax
Visual Basic
Public Property AutoPhase As Boolean
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objSheet As SolidEdgeDraft.Sheet
    Dim objCircle As SolidEdgeFrameworkSupport.Circle2d
    Dim objGeometricStyle As SolidEdgeFrameworkSupport.GeometryStyle2d
    Dim bAutoPhase As Boolean
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
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'getting the Active Sheet object
    Set objSheet = objDoc.ActiveSheet
    'Create a circle in the active sheet.
    Set objCircle = objSheet.Circles2d.AddByCenterRadius(x:=0.2, y:=0.2, _
                                                         Radius:=0.1)
    'Create a geometric style2d for the Circle
    Set objGeometricStyle = objCircle.Style
    'Get the AutoPhase status
    bAutoPhase = objGeometricStyle.AutoPhase
    'Set the AutoPhase to True
    objGeometricStyle.AutoPhase = True
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSheet = Nothing
    Set objCircle = Nothing
    Set objGeometricStyle = Nothing
End Sub
See Also

GeometryStyle2d Object  | GeometryStyle2d Members