Solid Edge FrameworkSupport Type Library
LinearName Property
Description
Sets and returns the linear style for the referenced object.
Property type
Read-write property
Syntax
Visual Basic
Public Property LinearName As String
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objSheet As SolidEdgeDraft.Sheet
    Dim objCircle As SolidEdgeFrameworkSupport.Circle2d
    Dim objGeometricStyle As SolidEdgeFrameworkSupport.GeometryStyle2d
    Dim strName As String
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
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'getting the Active Sheet object
    Set objSheet = objDoc.ActiveSheet
    objDoc.LinearStyles.Active = "Center"
    'Create a circle in the active sheet.
    Set objCircle = objSheet.Circles2d.AddByCenterRadius(x:=0.2, y:=0.2, _
                                                         Radius:=0.1)
    'Create a geometric style2d for the Circle
    Set objGeometricStyle = objCircle.Style
    'Get the Linearname of the Style
    strName = objGeometricStyle.LinearName
    'Set the Linear name to Cutting Plane
    objGeometricStyle.LinearName = "Cutting Plane"
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSheet = Nothing
    Set objCircle = Nothing
    Set objGeometricStyle = Nothing
End Sub
See Also

GeometryStyle2d Object  | GeometryStyle2d Members