Solid Edge FrameworkSupport Type Library
ClearStyle Method
Description
Clears any previously set style object.
Syntax
Visual Basic
Public Sub ClearStyle() 
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objSheet As SolidEdgeDraft.Sheet
    Dim objLeaders As SolidEdgeFrameworkSupport.Leaders
    Dim objANSIStyle As SolidEdgeFrameworkSupport.DimensionStyle
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
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'getting the Active Sheet object
    Set objSheet = objDoc.ActiveSheet
    'Create Leaders collection object
    Set objLeaders = objSheet.Leaders
    'Create a dimension style
    Set objANSIStyle = objDoc.DimensionStyles.Add(Name:="MyDimStyle", Parent:="ANSI")
    'Set the STyle to ANSI
    objLeaders.Style = objANSIStyle
    'Clear the Style of the Leaders object
    Call objLeaders.ClearStyle
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSheet = Nothing
    Set objLeaders = Nothing
    Set objANSIStyle = Nothing
End Sub
See Also

Leaders Collection  | Leaders Members