Solid Edge FrameworkSupport Type Library
Item Method
Variant (input) index.
Description
The items in a collection.
Syntax
Visual Basic
Public Function Item( _
   ByVal Index As Variant _
) As Leader
Parameters
Index
Variant (input) index.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objSheet As SolidEdgeDraft.Sheet
    Dim objTextBox As SolidEdgeFrameworkSupport.TextBoxes
    Dim objLeaders As SolidEdgeFrameworkSupport.Leaders
    Dim objLeader1 As SolidEdgeFrameworkSupport.Leader
    Dim objItem1 As SolidEdgeFrameworkSupport.Leader
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
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'getting the Active Sheet object
    Set objSheet = objDoc.ActiveSheet
    'Create Leaders collection object
    Set objLeaders = objSheet.Leaders
    'Create a leader attatched to text box
    Set objLeader1 = objLeaders.Add(x1:=0.1, y1:=0.1, z1:=0, x2:=0.1, y2:=0.3, z2:=0)
    'Get the item1
    Set objItem1 = objLeaders.Item(Index:=1)
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSheet = Nothing
    Set objTextBox = Nothing
    Set objLeaders = Nothing
    Set objLeader1 = Nothing
    Set objItem1 = Nothing
End Sub
See Also

Leaders Collection  | Leaders Members