Solid Edge FrameworkSupport Type Library
Style Property
Description
For collection objects, Body objects, RefPlane objects, Sketch objects, CoordinateSystem objects, CommandBarButton objects, SmartFrame2d objects, View objects, and TextCharStyle objects, Style is read-write. For all other objects, Style is read-only.
Property type
Read-write property
Syntax
Visual Basic
Public Property Style As DimensionStyle
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objSheet As SolidEdgeDraft.Sheet
    Dim objLeaders As SolidEdgeFrameworkSupport.Leaders
    Dim objANSIStyle As SolidEdgeFrameworkSupport.DimensionStyle
    Dim objStyle As SolidEdgeFrameworkSupport.DimensionStyle
    ' Report errors
    Const PI = 3.14159265358979
    ' Create/get the application with specific settings
    On Error Resume Next
    Set objApp = GetObject(, "SolidEdge.Application")
    If Err Then
        Err.Clear
        Set objApp = CreateObject("SolidEdge.Application")
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'getting the Active Sheet object
    Set objSheet = objDoc.ActiveSheet
    'Create Leaders collection object
    Set objLeaders = objSheet.Leaders
    'Create a dimension style
    Set objANSIStyle = objDoc.DimensionStyles.Add(Name:="MyDimStyle", Parent:="ANSI")
    'Set the STyle to ANSI
    objLeaders.Style = objANSIStyle
    'Get the Style associated with Leaders object
    Set objStyle = objLeaders.Style
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSheet = Nothing
    Set objLeaders = Nothing
    Set objANSIStyle = Nothing
    Set objStyle = Nothing
End Sub
See Also

Leaders Collection  | Leaders Members