Solid Edge FrameworkSupport Type Library
Cut Method
Description
Moves the referenced object to the system clipboard.
Syntax
Visual Basic
Public Sub Cut() 
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFrameWork.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objSheet As SolidEdgeDraft.Sheet
    Dim objLines2d As SolidEdgeFrameworkSupport.Lines2d
    Dim objLine1 As SolidEdgeFrameworkSupport.Line2d
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
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'getting the Active Sheet object
    Set objSheet = objDoc.ActiveSheet
    ' getting the lines2d collection object
    Set objLines2d = objSheet.Lines2d
    ' Create Line2d object using AddBy2Points method
    Set objLine1 = objLines2d.AddBy2Points(x1:=0.05, y1:=0.05, x2:=0.1, y2:=0.05)
    'Cut the line
    Call objLine1.Cut
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSheet = Nothing
    Set objLines2d = Nothing
    Set objLine1 = Nothing
End Sub
See Also

Line2d Object  | Line2d Members