Private Sub Form_Load()
Dim objApp As SolidEdgeFramework.Application
Dim objDoc As SolidEdgePart.PartDocument
Dim objLines As SolidEdgeFrameworkSupport.Lines2d
Dim objLine1 As SolidEdgeFrameworkSupport.Line2d
Dim xCoord As Double
Dim yCoord As Double
' Report errors
Const PI = 3.14159265358979
' Create/get the application with specific settings
On Error Resume Next
Set objApp = GetObject(, "SolidEdge.Application")
If Err Then
Err.Clear
Set objApp = CreateObject("SolidEdge.Application")
Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
objApp.Visible = True
Else
Set objDoc = objApp.ActiveDocument
End If
'Create an empty Lines2d collection object
Set objLines = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:=objDoc.RefPlanes(1)) _
.Lines2d
' Create a Line2d object
Set objLine1 = objLines.AddBy2Points(x1:=0, y1:=0, x2:=0.1, y2:=0.15)
'Get the EndPoint of the Line object
Call objLine1.GetEndPoint(x:=xCoord, y:=yCoord)
' USER DISPLAY
' Release objects
Set objApp = Nothing
Set objDoc = Nothing
Set objLines = Nothing
Set objLine1 = Nothing
End Sub