Private Sub Form_Load()
Dim objApp As SolidEdgeFrameWork.Application
Dim objDoc As SolidEdgeDraft.DraftDocument
Dim objSheet As SolidEdgeDraft.Sheet
Dim objLines2d As SolidEdgeFrameworkSupport.Lines2d
Dim objLine1 As SolidEdgeFrameworkSupport.Line2d
Dim objStyle1 As SolidEdgeFrameWork.LinearStyle
Dim objGetStyle As Object
Dim dblx1 As Double, dbly1 As Double, dblx2 As Double, dbly2 As Double
' Report errors
Const PI = 3.14159265358979
' Create/get the application with specific settings
On Error Resume Next
Set objApp = GetObject(, "SolidEdge.Application")
If Err Then
Err.Clear
Set objApp = CreateObject("SolidEdge.Application")
Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
objApp.Visible = True
Else
Set objDoc = objApp.ActiveDocument
End If
'getting the Active Sheet object
Set objSheet = objDoc.ActiveSheet
'get linear style object
Set objStyle1 = objDoc.LinearStyles(7)
' getting the lines2d collection object
Set objLines2d = objSheet.Lines2d
' Create Line2d object using AddBy2Points method
Set objLine1 = objLines2d.AddBy2Points(x1:=0.05, y1:=0.05, x2:=0.1, y2:=0.05)
' add segment style to the line2d object
Call objLine1.AddSegmentedStyle(x1:=0.05, y1:=0.05, x2:=0.1, _
y2:=0.05, Style:=objStyle1)
'get Segemented style
Call objLine1.GetSegmentedStyle(Index:=1, x1:=dblx1, y1:=dbly1, x2:=dblx2, y2:=dbly2, Style:=objGetStyle)
' USER DISPLAY
' Release objects
Set objApp = Nothing
Set objDoc = Nothing
Set objSheet = Nothing
Set objLines2d = Nothing
Set objLine1 = Nothing
Set objStyle1 = Nothing
End Sub