Solid Edge FrameworkSupport Type Library
RemoveAllSegmentedStyles Method
Description
Removes all segments defined for the referenced graphic object.
Syntax
Visual Basic
Public Sub RemoveAllSegmentedStyles() 
Remarks
Removing segmented styles does not remove the geometry. Instead, it removes the linear styles applied to the graphic object defined by the segments. If a segment is blank (for example, when the linear style is null), it reappears when its segment is removed.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFrameWork.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objSheet As SolidEdgeDraft.Sheet
    Dim objLines2d As SolidEdgeFrameworkSupport.Lines2d
    Dim objLine1 As SolidEdgeFrameworkSupport.Line2d
    Dim objStyle1 As SolidEdgeFrameWork.LinearStyle
    Dim objStyle2 As SolidEdgeFrameWork.LinearStyle
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
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'getting the Active Sheet object
    Set objSheet = objDoc.ActiveSheet
    ' getting the lines2d collection object
    Set objLines2d = objSheet.Lines2d
    ' Create Line2d object using AddBy2Points method
    Set objLine1 = objLines2d.AddBy2Points(x1:=0.05, y1:=0.05, x2:=0.1, y2:=0.05)
    'get 2nos linear style object
    Set objStyle1 = objDoc.LinearStyles(3)
    Set objStyle2 = objDoc.LinearStyles.Add(Name:="LinearStyleDotted", _
                                            Parent:="Dotted")
    'Add first SegmentedStyle
    Call objLine1.AddSegmentedStyle(x1:=0.05, y1:=0.05, x2:=0.08, _
                                    y2:=0.05, Style:=objStyle1)
    'Add second SegmentedStyle
    Call objLine1.AddSegmentedStyle(x1:=0.08, y1:=0.05, x2:=0.1, _
                                    y2:=0.05, Style:=objStyle2)
    'remove all segmented styles
    Call objLine1.RemoveAllSegmentedStyles
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSheet = Nothing
    Set objLines2d = Nothing
    Set objLine1 = Nothing
    Set objStyle1 = Nothing
    Set objStyle2 = Nothing
End Sub
See Also

Line2d Object  | Line2d Members