Private Sub Form_Load()
Dim objApp As SolidEdgeFramework.Application
Dim objDoc As SolidEdgePart.PartDocument
Dim objLines As SolidEdgeFrameworkSupport.Lines2d
Dim objLine1 As SolidEdgeFrameworkSupport.Line2d
Dim objLine2 As SolidEdgeFrameworkSupport.Line2d
Dim sDumpStatus As String ' Used for temporary storage of datadump return string
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
Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
objApp.Visible = True
Else
Set objDoc = objApp.ActiveDocument
End If
'Create Lines collection object
Set objLines = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:= _
objDoc.RefPlanes(1)).Lines2d
'Create a Line object
Set objLine1 = objLines.AddBy2Points(x1:=0, y1:=0, x2:=0.1, y2:=0)
' Select the Line object
' Set objLine2 = objLine1.Select
Call objLine1.Select
' USER DISPLAY
' Release objects
Set objApp = Nothing
Set objDoc = Nothing
Set objLines = Nothing
Set objLine1 = Nothing
Set objLine2 = Nothing
End Sub