Solid Edge FrameworkSupport Type Library
Rotate Method
Specifies, in radians, the angle of rotation.
Specifies the x coordinate for the point of rotation.
Specifies the y coordinate for the point of rotation.
Description
Rotates the referenced object about the point specified by the angle in radians.
Syntax
Visual Basic
Public Sub Rotate( _
   ByVal Angle As Double, _
   ByVal x As Double, _
   ByVal y As Double _
) 
Parameters
Angle
Specifies, in radians, the angle of rotation.
x
Specifies the x coordinate for the point of rotation.
y
Specifies the y coordinate for the point of rotation.
Remarks
If the object is to be rotated about its center point, the origin must be set to its center point.
See Also

LineString2d Object  | LineString2d Members