Solid Edge FrameworkSupport Type Library
Item Method
Variant (input) index.
Description
The items in a collection.
Syntax
Visual Basic
Public Function Item( _
   ByVal Index As Variant _
) As LineString2d
Parameters
Index
Variant (input) index.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objSheet As SolidEdgeDraft.Sheet
    Dim objLineStrings As SolidEdgeFrameworkSupport.LineStrings2d
    Dim objLineString1 As SolidEdgeFrameworkSupport.LineString2d
    Dim objLineString2 As SolidEdgeFrameworkSupport.LineString2d
    Dim dblPoint(1 To 8) As Double
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
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    ' Get the Sheet object
    Set objSheet = objDoc.Sheets(1)
    ' Get the LineStrings2d collection object
    Set objLineStrings = objSheet.LineStrings2d
    'Assign the value to Points array
    dblPoint(1) = 0.1
    dblPoint(2) = 0.1
    dblPoint(3) = 0.2
    dblPoint(4) = 0.1
    dblPoint(5) = 0.2
    dblPoint(6) = 0.2
    dblPoint(7) = 0.1
    dblPoint(8) = 0.2
    ' Create a LineString2d object
    Set objLineString1 = objLineStrings.AddByPoints(PointCount:=4, Points:=dblPoint)
    'Get a another reference to the LineString object with Item method
    Set objLineString2 = objLineStrings.Item(Index:=1)
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSheet = Nothing
    Set objLineStrings = Nothing
    Set objLineString1 = Nothing
    Set objLineString2 = Nothing
End Sub
See Also

LineStrings2d Collection  | LineStrings2d Members