Solid Edge FrameworkSupport Type Library
BringForward Method
Description
Changes the display order of the referenced object by moving it in front of the first object that obscures it.
Syntax
Visual Basic
Public Sub BringForward() 
Remarks
This command is useful when other objects that are filled hide an object and the user wants to remove the object from hiding while not bringing the object to the top of the priority list.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFrameWork.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objSheet As SolidEdgeDraft.Sheet
    Dim objPoints As SolidEdgeFrameworkSupport.Points2d
    Dim objPoint1 As SolidEdgeFrameworkSupport.Point2d
    Dim objPoint2 As SolidEdgeFrameworkSupport.Point2d
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
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'getting the Active Sheet object
    Set objSheet = objDoc.ActiveSheet

    'create Points collection
    Set objPoints = objSheet.Points2d
    'Create a Point
    Set objPoint1 = objPoints.Add(x:=0.25, y:=0.25)
    'Create one more Point
    Set objPoint2 = objPoints.Add(x:=0.25, y:=0.25)

    'use BringForward method
    objPoint1.BringForward


    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSheet = Nothing
    Set objPoints = Nothing
    Set objPoint1 = Nothing
    Set objPoint2 = Nothing
End Sub
See Also

Point2d Object  | Point2d Members