Solid Edge FrameworkSupport Type Library
GetKeyPoint Method
Specifies the index of the keypoint/handle.
X coordinate of the specified keypoint.
Y coordinate of the specified keypoint.
Z coordinate of the specified keypoint.
Returns a member of the KeyPointType constant set.
Returns a value in the HandleType constant set.
Description
Returns information about a specified key point.
Syntax
Visual Basic
Public Sub GetKeyPoint( _
   ByVal Index As Long, _
   ByRef x As Double, _
   ByRef y As Double, _
   ByRef z As Double, _
   ByRef KeypointType As KeyPointType, _
   ByRef HandleType As Long _
) 
Parameters
Index
Specifies the index of the keypoint/handle.
x
X coordinate of the specified keypoint.
y
Y coordinate of the specified keypoint.
z
Z coordinate of the specified keypoint.
KeypointType
ValueDescription
igKeyPointCallbackKeypoint Type - Callback
igKeyPointCenterKeypoint Type - Center
igKeyPointEndKeypoint Type - End
igKeyPointHorizontalSilhouetteKeypoint Type - Horizontal Silhouette
igKeyPointInteriorNodeKeypoint Type - Interior Node
igKeyPointInteriorPoleKeypoint Type - Interior Pole
igKeyPointMajorAxisKeypoint Type - Major Axis
igKeyPointMiddleKeypoint Type - Middle
igKeyPointMinorAxisKeypoint Type - Minor Axis
igKeyPointNonDefiningKeypoint Type - Non-defining
igKeyPointPointOnlyKeypoint Type - Point Only
igKeyPointStartKeypoint Type - Start
igKeyPointVerticalSilhouetteKeypoint Type - Vertical Silhouette
Returns a member of the KeyPointType constant set.
HandleType
Returns a value in the HandleType constant set.
Remarks
The key point is specified by its index.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFrameWork.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objSheet As SolidEdgeDraft.Sheet
    Dim objPoints As SolidEdgeFrameworkSupport.Points2d
    Dim objPoint As SolidEdgeFrameworkSupport.Point2d
    Dim dblXPoint As Double
    Dim dblYPoint As Double
    Dim dblZPoint As Double
    Dim lngKPType As Long
    Dim lngKPHandle As Long
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
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'getting the Active Sheet object
    Set objSheet = objDoc.ActiveSheet

    'create a Points collection.
    Set objPoints = objSheet.Points2d
    'create a Point
    Set objPoint = objPoints.Add(x:=0.25, y:=0.25)
    'call GetKeyPoint method.
    Call objPoint.GetKeyPoint(Index:=0, x:=dblXPoint, y:=dblYPoint, z:=dblZPoint, KeyPointType:=lngKPType, HandleType:=lngKPHandle)





    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSheet = Nothing
    Set objPoints = Nothing
    Set objPoint = Nothing
End Sub
See Also

Point2d Object  | Point2d Members