Solid Edge FrameworkSupport Type Library
GetPoint Method
Coordinates of the referenced point object.
Coordinates of the referenced point object.
Description
Returns the coordinates of the referenced Point2d object.
Syntax
Visual Basic
Public Sub GetPoint( _
   ByRef x As Double, _
   ByRef y As Double _
) 
Parameters
x
Coordinates of the referenced point object.
y
Coordinates of the referenced point object.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFrameWork.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objSheet As SolidEdgeDraft.Sheet
    Dim objPoints As solidedgeframeworksupport.Points2d
    Dim objPoint As solidedgeframeworksupport.Point2d
    Dim dblX As Double
    Dim dblY As Double
    ' Dim dblZ As Double
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
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'getting the Active Sheet object
    Set objSheet = objDoc.ActiveSheet
    'create a Points collection
    Set objPoints = objSheet.Points2d
    'create Point
    Set objPoint = objPoints.Add(x:=0.25, y:=0.25)
    'Call GetPoint method.
    Call objPoint.GetPoint(dblX, dblY)



    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSheet = Nothing
    Set objPoints = Nothing
    Set objPoint = Nothing
End Sub
See Also

Point2d Object  | Point2d Members