Solid Edge FrameworkSupport Type Library
Key Property
Description
Returns a key (a string) to find the object relative to its owning parents.
Property type
Read-only property
Syntax
Visual Basic
Public Property Key( _
   Optional ByVal Recurse As Variant _
) As String
Parameters
Recurse
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFrameWork.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objSheet As SolidEdgeDraft.Sheet
    Dim objPoints As SolidEdgeFrameworkSupport.Points2d
    Dim objPoint As SolidEdgeFrameworkSupport.Point2d
    Dim sKey As String
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
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'getting the Active Sheet object
    Set objSheet = objDoc.ActiveSheet
    'Create Points collection
    Set objPoints = objSheet.Points2d
    'Create a point
    Set objPoint = objPoints.Add(0.25, 0.25)
    'get Key
    sKey = objPoint.Key(False)

    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSheet = Nothing
    Set objPoints = Nothing
    Set objPoint = Nothing
End Sub
See Also

Point2d Object  | Point2d Members