Solid Edge FrameworkSupport Type Library
SendToBack Method
Description
Changes the display order of visible objects by moving the referenced object behind all overlapping objects.
Syntax
Visual Basic
Public Sub SendToBack() 
Remarks
This command is useful when objects are hiding other objects that have a lower priority display. The SendBackward method can also be used.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFrameWork.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objSheet As SolidEdgeDraft.Sheet
    Dim objPoints As SolidEdgeFrameworkSupport.Points2d
    Dim objPoint1 As SolidEdgeFrameworkSupport.Point2d
    Dim objPoint2 As SolidEdgeFrameworkSupport.Point2d
    Dim objPoint3 As SolidEdgeFrameworkSupport.Point2d
    Dim lngPoint1Zorder As Long, lngPoint2Zorder As Long, lngPoint3Zorder As Long
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
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'getting the Active Sheet object
    Set objSheet = objDoc.ActiveSheet
    'create Points collection
    Set objPoints = objSheet.Points2d
    'Create Points
    Set objPoint1 = objPoints.Add(x:=0.25, y:=0.25)
    Set objPoint2 = objPoints.Add(x:=0.25, y:=0.3)
    Set objPoint3 = objPoints.Add(x:=0.3, y:=0.3)
    'SendToBack
    Call objPoint3.SendToBack

    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSheet = Nothing
    Set objPoints = Nothing
    Set objPoint1 = Nothing
    Set objPoint2 = Nothing
    Set objPoint3 = Nothing
End Sub
See Also

Point2d Object  | Point2d Members