Solid Edge FrameworkSupport Type Library
Width Property
Description
Returns the width of the referenced object.
Property type
Read-write property
Syntax
Visual Basic
Public Property Width As Double
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objProfile As SolidEdgePart.Profile
    Dim objRPattern As SolidEdgeFrameworkSupport.RectangularPattern2d
    Dim dblWidth As Double
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    ' Create a new Profile object
    Set objProfile = objDoc.ProfileSets.Add.Profiles.Add(objDoc.RefPlanes(1))
    ' Create a RectangularPattern2d object on the profile
    Set objRPattern = objProfile.RectangularPatterns2d.Add(OriginX:=0, OriginY:=0, _
                                                           Width:=0.1, Height:=0.05, Angle:=0, OffsetType:=sePatternFillOffset, _
                                                           XCount:=6, YCount:=4, XSpace:=0.015, YSpace:=0.01)
    ' Get and change the width of the RectangularPattern2d object
    dblWidth = objRPattern.Width
    objRPattern.Width = 0.15
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objProfile = Nothing
    Set objRPattern = Nothing
End Sub
See Also

RectangularPattern2d Object  | RectangularPattern2d Members