Private Sub Form_Load()
Dim objApp As SolidEdgeFramework.Application
Dim objDoc As SolidEdgePart.PartDocument
Dim objCirc1 As SolidEdgeFrameworkSupport.Circle2d
Dim objCirc2 As SolidEdgeFrameworkSupport.Circle2d
Dim objRelns As SolidEdgeFrameworkSupport.Relations2d
Dim objReln1 As SolidEdgeFrameworkSupport.Relation2d
Dim objProfile As SolidEdgePart.Profile
' Report errors
Const PI = 3.14159265358979
' Create/get the application with specific settings
On Error Resume Next
Set objApp = GetObject(, "SolidEdge.Application")
If Err Then
Err.Clear
Set objApp = CreateObject("SolidEdge.Application")
Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
objApp.Visible = True
Else
Set objDoc = objApp.ActiveDocument
End If
' Create an empty Profile
Set objProfile = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:= _
objDoc.RefPlanes(1))
' Create 2 Circle objects
Set objCirc1 = objProfile.Circles2d.AddByCenterRadius(x:=0, y:=0, Radius:=0.1)
Set objCirc2 = objProfile.Circles2d.AddByCenterRadius(x:=0.05, y:=0.05, Radius:=0.12)
' Create a Concentric Relation between the objects
Set objRelns = objProfile.Relations2d
Set objReln1 = objRelns.AddConcentric(Object1:=objCirc1, Object2:=objCirc2)
' Delete the Relation2d object
Call objReln1.Delete
' USER DISPLAY
' Release objects
Set objApp = Nothing
Set objDoc = Nothing
Set objCirc1 = Nothing
Set objCirc2 = Nothing
Set objRelns = Nothing
Set objProfile = Nothing
Set objReln1 = Nothing
End Sub