Solid Edge FrameworkSupport Type Library
ZOrder Property
Description
Specifies the front-to-back order in which an object is displayed relative to other objects.
Property type
Read-only property
Syntax
Visual Basic
Public Property ZOrder As Long
Remarks
This relationship is maintained by storing a cardinal order position on each object. An object with a higher cardinal order is displayed in front of one with a lower cardinal number. A change in an object's ZOrder changes how objects are displayed if filled objects are displayed over other objects. The value assigned to this property can be changed internally to maintain unique values on all objects. Therefore, the value returned for this property may not be the same value to which the property was set.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFrameWork.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objLine1 As SolidEdgeFrameworkSupport.Line2d
    Dim objLine2 As SolidEdgeFrameworkSupport.Line2d
    Dim objRelns As SolidEdgeFrameworkSupport.Relations2d
    Dim objReln1 As SolidEdgeFrameworkSupport.Relation2d
    Dim objSheet As SolidEdgeDraft.Sheet
    Dim lngZOrder As Long
    ' Report errors
    Const PI = 3.14159265358979
    ' Create/get the application with specific settings
    On Error Resume Next
    Set objApp = GetObject(, "SolidEdge.Application")
    If Err Then
        Err.Clear
        Set objApp = CreateObject("SolidEdge.Application")
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    ' Get the active sheet
    Set objSheet = objDoc.ActiveSheet
    ' Create 2 Line objects
    Set objLine1 = objSheet.Lines2d.AddBy2Points(x1:=0.05, y1:=0.025, x2:=0.05, y2:=0.05)
    Set objLine2 = objSheet.Lines2d.AddBy2Points(x1:=0.05, y1:=0.1, x2:=0.075, y2:=0.075)

    ' Create a Parallel Relation between the objects
    Set objRelns = objSheet.Relations2d
    Set objReln1 = objRelns.AddParallel(Object1:=objLine1, Object2:=objLine2, guaranteed_ok:=True)
    ' Get the ZOrder property
    lngZOrder = objReln1.ZOrder
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objLine1 = Nothing
    Set objLine2 = Nothing
    Set objRelns = Nothing
    Set objSheet = Nothing
    Set objReln1 = Nothing
End Sub
See Also

Relation2d Object  | Relation2d Members