Solid Edge FrameworkSupport Type Library
AddHorizontalAlign Method
Specifies the first object to which the constraint is to be applied.
Specifies the key point index of Object1.
Specifies the second object to which the constraint is to be applied.
Specifies the key point index of Object2.
If set, checking is performed to ensure that the relationship does not contradict previously placed relationships.
Description
Adds a horizontal alignment relationship to a Relations2d collection.
Syntax
Visual Basic
Public Function AddHorizontalAlign( _
   ByVal Object1 As Object, _
   ByVal Index1 As Long, _
   ByVal Object2 As Object, _
   ByVal Index2 As Long, _
   Optional ByVal guaranteed_ok As Variant _
) As Relation2d
Parameters
Object1
Specifies the first object to which the constraint is to be applied.
Index1
Specifies the key point index of Object1.
Object2
Specifies the second object to which the constraint is to be applied.
Index2
Specifies the key point index of Object2.
guaranteed_ok
If set, checking is performed to ensure that the relationship does not contradict previously placed relationships.
Remarks
The method aligns the first specified key point to be horizontal to the second specified key point. Relationship Add methods have checks to ensure that a new relationship does not contradict previously placed relationships. For example, AddHorizontal will return an error if the line already has a vertical relationship. This check can be turned off to enhance performance. The optional “guaranteed_ok” argument, if set to 1, bypasses relationship checking. However, this feature could leave the system in an unsolvable state, so use it with extreme caution. It is best to use this feature only on a new element with no other relationships.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objCirc1 As SolidEdgeFrameworkSupport.Circle2d
    Dim objCirc2 As SolidEdgeFrameworkSupport.Circle2d
    Dim objRelns As SolidEdgeFrameworkSupport.Relations2d
    Dim objReln1 As SolidEdgeFrameworkSupport.Relation2d
    Dim objProfile As SolidEdgePart.Profile
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If

    ' Create an empty Profile
    Set objProfile = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:= _
                                                         objDoc.RefPlanes(1))
    ' Create 2 Circle objects
    Set objCirc1 = objProfile.Circles2d.AddByCenterRadius(x:=0, y:=0, Radius:=0.05)
    Set objCirc2 = objProfile.Circles2d.AddByCenterRadius(x:=0.1, y:=0.1, Radius:=0.05)

    ' Create a HorizontalAlign Relation between the objects
    Set objRelns = objProfile.Relations2d
    Set objReln1 = objRelns.AddHorizontalAlign(Object1:=objCirc1, Index1:=0, _
                                               Object2:=objCirc2, Index2:=0)

    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objCirc1 = Nothing
    Set objCirc2 = Nothing
    Set objProfile = Nothing
    Set objRelns = Nothing
    Set objReln1 = Nothing
End Sub
See Also

Relations2d Collection  | Relations2d Members