Private Sub Form_Load()
Dim objApp As SolidEdgeFramework.Application
Dim objDoc As SolidEdgePart.PartDocument
Dim objLines As SolidEdgeFrameworkSupport.Lines2d
Dim objLine1 As SolidEdgeFrameworkSupport.Line2d
Dim objLine2 As SolidEdgeFrameworkSupport.Line2d
Dim objLine3 As SolidEdgeFrameworkSupport.Line2d
Dim objRelns As SolidEdgeFrameworkSupport.Relationships2d
Dim objRelns2 As SolidEdgeFrameworkSupport.Relation2d
Dim lngCnt As Long
' Report errors
Const PI = 3.14159265358979
' Create/get the application with specific settings
On Error Resume Next
Set objApp = GetObject(, "SolidEdge.Application")
If Err Then
Err.Clear
Set objApp = CreateObject("SolidEdge.Application")
Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
objApp.Visible = True
Else
Set objDoc = objApp.ActiveDocument
End If
'Create an empty Lines2d collection object
Set objLines = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:= _
objDoc.RefPlanes(1)).Lines2d
' Create 2 Line2d objects
Set objLine1 = objLines.AddBy2Points(x1:=0, y1:=0, x2:=0.1, y2:=0)
Set objLine2 = objLines.AddBy2Points(x1:=0.1, y1:=0, x2:=0.1, y2:=0.1)
' Create another Line object using the AddAsChamfer Method
Set objLine3 = objLines.AddAsChamfer(Obj1:=objLine1, Obj2:=objLine2, xDirection:=1, _
yDirection:=1, SetBackA:=0.04, SetBackB:=0.03)
' Get the Relationships of the Line object
Set objRelns = objLine3.Relationships
If objRelns(1).Type <> igChamferRelation2d Then
MsgBox ("Error in the Relationships Property of Line2d object")
End If
' Create a Relationships2d object using item method
Set objRelns2 = objRelns.Item(1)
' USER DISPLAY
' Release objects
Set objApp = Nothing
Set objDoc = Nothing
Set objLines = Nothing
Set objLine1 = Nothing
Set objLine2 = Nothing
Set objLine3 = Nothing
Set objRelns = Nothing
Set objRelns2 = Nothing
End Sub