Solid Edge FrameworkSupport Type Library : SmartFrame2dDefaults Object |
![]() | Returns the origin for the referenced object. |
![]() | Redefines the offset between the lower left corner of the window and the object's origin. |
![]() | Specifies whether or not the contents of the referenced SmartFrame object are to be displayed. |
![]() | Sets and returns the distance from the origin of the referenced object to the bottom of the frame or view. |
![]() | Sets and returns the distance from the origin of the referenced object to the left side of the frame or view. |
![]() | Sets and returns the distance from the origin of the referenced object to the right side of the frame or view. |
![]() | Sets and returns the distance from the origin of the referenced object to the top of the frame or view. |
![]() | Specifies whether or not the file associated with the referenced SmartFrame object is public. |
![]() | Specifies whether or not the referenced object can be selected by a mouse click. |
![]() | For OLE objects, specifies the angle at which the object is rotated along its major axis. For hatch lines, sets and returns the rotation angle used to display hatch lines. |
![]() | Sets and returns the scale factor between an object and its source document. |
![]() | Sets and returns the update status of an OLE object when the source is modified. |