Solid Edge FrameworkSupport Type Library
LocateChildren Property
Description
Specifies whether or not the associated SmartFrame can be located by a spot anywhere within the range of the SmartFrame.
Property type
Read-write property
Syntax
Visual Basic
Public Property LocateChildren As Boolean
Remarks
If this property True, the SmartFrame2d can be located only by identifying the frame or the object within the frame. If False, the SmartFrame2d can be located by identifying a spot anywhere within the range of the SmartFrame2d - not necessarily on an element of the object.
See Also

SmartFrame2dStyle Object  | SmartFrame2dStyle Members