Solid Edge FrameworkSupport Type Library
Margin Property
Description
Sets and returns the minimum distance from the extents of the OLE object to the extents of the frame boundary.
Property type
Read-write property
Syntax
Visual Basic
Public Property Margin As Double
Remarks
The distance is specified in container units.
See Also

SmartFrame2dStyle Object  | SmartFrame2dStyle Members