Solid Edge FrameworkSupport Type Library
Printed Property
Collapse All
Expand All
Solid Edge FrameworkSupport Type Library
>
SmartFrame2dStyle Object
: Printed Property
Description
Specifies whether or not the OLE object (and its frame) is printed when the container is printed.
Property type
Read-write property
Syntax
Visual Basic
Public Property Printed As Boolean
Remarks
This is useful for objects such as sound clips that use an icon representation.
See Also
SmartFrame2dStyle Object
|
SmartFrame2dStyle Members