Solid Edge FrameworkSupport Type Library
SizeMode Property
Collapse All
Expand All
Solid Edge FrameworkSupport Type Library
>
SmartFrame2dStyle Object
: SizeMode Property
Description
Sets and returns the mode that defines what the frame should do when the OLE object's extents change.
Property type
Read-write property
Syntax
Visual Basic
Public Property SizeMode As
SizeModeConstants
Remarks
If the frame is currently cropping the object, this mode is not used, and the frame continues to crop the object. Valid values are members of the SizeModeConstants constant set.
See Also
SmartFrame2dStyle Object
|
SmartFrame2dStyle Members