AllAround | |
AllAroundLeaderSymbol | Display all around symbol for Surface Finish Symbol at the connect point of the leader line and break line. |
Application | Returns the active application object. |
AttributeSets | Returns the AttributeSets collection object for the referenced object. |
BreakLine | Specifies whether or not a breakline is added between the leader line and the referenced dimensioning object. |
BreakLineDirection | Sets and returns the direction (left or right) in which the break line runs along the x axis. |
BreakLineDistance | Sets and returns the length along the x axis that the break line traverses. |
CompressSymbolSize | Compress the size of Surface Finish Symbol so that the symbol height will be reduced for a single line. |
Document | Returns the document to which the referenced object belongs. |
HidePMI | Show or Hide the referenced PMI Surface Finish Symbol object. |
Index | Returns the numeric index for the active object. |
IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. |
Key | Returns a key (a string) to find the object relative to its owning parents. |
KeyPointCount | Returns the number of keypoints/handles that are supported by the referenced object. |
Layer | Sets and returns the named layer on which the referenced object resides. |
Leader | Specifies whether or not the referenced object has a leader line. |
MachiningAllowance | Sets and returns the machining allowance value text used in the referenced object. |
Name | Returns the name of the referenced object. |
Parent | Returns the parent object for the referenced object. |
Plane | For dimensions, returns the planar object used by the dimension to measure an object. For profiles, CopiedPart objects, and CopyConstruction objects, sets and returns the associated RefPlane object. |
PMIName | Get and set the name of reference PMI annotation object. |
PMIPlane | |
PMITrackDistance | |
ProductionMethod | Sets and returns the text used to specify the method of production as displayed in the referenced SurfaceFinishSymbol object. |
Requirements | |
RotationAngle | Sets and returns the angle, in radians, at which the object is rotated along its major axis. |
RoughnessValue | |
Style | For collection objects, Body objects, RefPlane objects, Sketch objects, CoordinateSystem objects, CommandBarButton objects, SmartFrame2d objects, View objects, and TextCharStyle objects, Style is read-write. For all other objects, Style is read-only. |
SurfaceFinishSymbol | Sets and returns the symbol used in the referenced SurfaceFinishSymbol object. |
SurfaceLaySymbol | Sets and returns the Surface Lay symbol used in the referenced SurfaceFinishSymbol object. |
TextScale | Sets and returns the text scale of the object. |
Type | Specifies the type of the object being referenced. |
VertexCount | Returns the number of vertices in the referenced object. |
ZOrder | Specifies the front-to-back order in which an object is displayed relative to other objects. |