Solid Edge FrameworkSupport Type Library
DataSet Property
Description
Sets and returns a previously saved set of property settings to apply to newly created annotation objects.
Property type
Write-only property
Syntax
Visual Basic
Public Property DataSet 
Remarks
These settings include the roughness value text, the active surface finish symbol, and so forth. The dimension style and leader on-off settings are not part of the data set.
See Also

SurfaceFinishSymbols Collection  | SurfaceFinishSymbols Members