Solid Edge FrameworkSupport Type Library
Add Method
Specifies the x coordinate for the new object.
Specifies the y coordinate for the new object.
Specifies the z coordinate for the new object.
Description
Adds an occurrence of the referenced object.
Syntax
Visual Basic
Public Function Add( _
   ByVal x1 As Double, _
   ByVal y1 As Double, _
   ByVal z1 As Double _
) As TextBox
Parameters
x1
Specifies the x coordinate for the new object.
y1
Specifies the y coordinate for the new object.
z1
Specifies the z coordinate for the new object.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objSheet As SolidEdgeDraft.Sheet
    Dim objTxtboxs As SolidEdgeFrameworkSupport.TextBoxes
    Dim objTxtbox As SolidEdgeFrameworkSupport.TextBox
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
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'get the Active Sheet object
    Set objSheet = objDoc.ActiveSheet
    ' Create a TextBox object
    Set objTxtboxs = objSheet.TextBoxes
    Set objTxtbox = objTxtboxs.Add(x1:=0.1, y1:=0.2, z1:=0)
    objTxtbox.Text = "Test1"
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSheet = Nothing
    Set objTxtboxs = Nothing
    Set objTxtbox = Nothing
End Sub
See Also

TextBoxes Collection  | TextBoxes Members