Solid Edge FrameworkSupport Type Library
Count Property
Description
Returns the number of objects in the referenced collection.
Property type
Read-only property
Syntax
Visual Basic
Public Property Count As Long
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objSheet As SolidEdgeDraft.Sheet
    Dim objTxtboxs As SolidEdgeFrameworkSupport.TextBoxes
    Dim objTxtbox As SolidEdgeFrameworkSupport.TextBox
    Dim objTxtbox1 As SolidEdgeFrameworkSupport.TextBox
    Dim lngCount As Long
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
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'get the Active Sheet object
    Set objSheet = objDoc.ActiveSheet
    'get the Txtboxs collection
    Set objTxtboxs = objSheet.TextBoxes
    'create 2 Textboxs by AddByTwoPoints method
    Set objTxtbox = objTxtboxs.AddByTwoPoints(x1:=0.1, y1:=0.1, z1:=0, _
                                              x2:=0.2, y2:=0.2, z2:=0)
    objTxtbox.Text = "Test box"
    Set objTxtbox1 = objTxtboxs.AddByTwoPoints(x1:=0.4, y1:=0.4, z1:=0, _
                                               x2:=0.5, y2:=0.5, z2:=0)
    objTxtbox1.Text = "Test box1"
    'Get the Count
    lngCount = objTxtboxs.Count

    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSheet = Nothing
    Set objTxtboxs = Nothing
    Set objTxtbox = Nothing
    Set objTxtbox1 = Nothing
End Sub
See Also

TextBoxes Collection  | TextBoxes Members