Solid Edge FrameworkSupport Type Library
Item Method
Variant (input) index.
Description
The items in a collection.
Syntax
Visual Basic
Public Function Item( _
   ByVal Index As Variant _
) As TextBox
Parameters
Index
Variant (input) index.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objSheet As SolidEdgeDraft.Sheet
    Dim objTxtboxs As SolidEdgeFrameworkSupport.TextBoxes
    Dim objTxtbox As SolidEdgeFrameworkSupport.TextBox
    Dim objTitem As SolidEdgeFrameworkSupport.TextBox
    ' Report errors
    Const PI = 3.14159265358979
    ' Create/get the application with specific settings
    On Error Resume Next
    Set objApp = GetObject(, "SolidEdge.Application")
    If Err Then
        Err.Clear
        Set objApp = CreateObject("SolidEdge.Application")
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'get the Active Sheet object
    Set objSheet = objDoc.ActiveSheet
    'get the Txtboxs collection
    Set objTxtboxs = objSheet.TextBoxes
    'create the Txtbox by AddByTwoPoints method
    Set objTxtbox = objTxtboxs.AddByTwoPoints(x1:=0.1, y1:=0.1, z1:=0, _
                                              x2:=0.2, y2:=0.2, z2:=0)
    'Get the object through Item method
    Set objTitem = objTxtboxs.Item(Index:=1)

    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSheet = Nothing
    Set objTxtboxs = Nothing
    Set objTxtbox = Nothing
    Set objTitem = Nothing
End Sub
See Also

TextBoxes Collection  | TextBoxes Members