AnchorPointLocation | Sets and returns the anchor point location of the referenced TextProfile object. |
Application | Returns the active application object. |
AttributeSets | Returns the AttributeSets collection object for the referenced object. |
FontName | Sets and returns the name of the font. |
IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. |
LetterSpacing | Sets and returns the spacing between letters for the associated text. |
LineSpacing | Sets and returns the spacing between lines for the associated text. |
Margin | Sets and returns the margin of the associated text. |
Parent | Returns the parent object for the referenced object. |
Smoothness | Sets and returns the smoothness of the associated text. Range is [100,4500], where 100 is smoothest and 4500 is coarsest. |
Text | Sets and returns the text of the referenced TextProfile object. |
TextSize | Sets and returns the size of the associated text. |