Solid Edge FrameworkSupport Type Library
Tail Property
Description
Specifies whether the less than symbol appears at the end of the breaklline.
Property type
Read-write property
Syntax
Visual Basic
Public Property Tail As DimWeldTailTypeConstants
Remarks
If this symbol is included, the Tail property also specifies if the symbol is open or closed.
See Also

WeldSymbolDataSet Object  | WeldSymbolDataSet Members