| Class Module | Description |
| Accelerator | Represents a collection of KeyBinding objects. |
| Accelerators | Represents a collection of Accelerator objects. |
| AddIn | A control that represents a command added to Solid Edge through the AddIn interface. |
| AddInEdgeBarEvents | |
| AddInEvents | A collection of AddInEvent objects. |
| AddIns | A collection of AddIn objects. |
| Application | Provides the properties and methods necessary for a Visual Basic user to drive Solid Edge programmatically. |
| ApplicationEvents | Fires application events. |
| ApplicationV8DocumentOpenEvent | Fires document open event |
| ApplicationWindowEvents | Provides access to the application window events. |
| AssemblyChangeEvents | Assembly change events. |
| AssemblyFamilyEvents | |
| AssemblyRecomputeEvents | Represents a collection of assembly recompute events. |
| Attribute | Represents an occurrence of a user-defined attribute. |
| AttributeQuery | Contains the QueryByName method, which enables you to locate attribute sets and individual attributes. |
| AttributeSet | Represents an occurrence of a user-defined attribute set. |
| AttributeSets | Represents a collection of AttributeSet objects. |
| BlockTableEvents | Contains the AfterUpdate event. |
| Command | Provides interfaces for Visual Basic users to capture user input to process Solid Edge events. |
| CommandBar | Represents all menus, toolbars, and pop-up menus in Solid Edge. |
| CommandBarButton | Represents buttons on toolbars and menus. |
| CommandBarButtonEvents | A collection of CommandBarButtonEvent objects. |
| CommandBarControl | Contains the properties and methods that are applicable to both CommandBarButton and CommandBarPopup objects. |
| CommandBarControls | Contains all of the buttons and pop-ups on a specific command bar. |
| CommandBarPopup | Represents pop-ups on toolbars and menus. |
| CommandBars | A collection of all of the command bars within a specific environment. |
| CommandCategories | A collection of command categories |
| CommandCategory | |
| CommandInfo | |
| CommandWindow | Triggers Command Window events. |
| ConnectorTableEvents | Contains the AfterUpdate event. |
| CPDInitializer | |
| CPDInitializerInsightXT | |
| Customization | An object that is sued to Customize the UI |
| DashStyle | The DashStyle object represents a custom dash style in a Draft document. |
| DashStyles | The DashStyles object represents a collection of DashStyle objects. |
| DISEAddInEvents | A collection of AddInEvent objects. |
| DISEAddInEventsEx | A collection of AddInEvent objects. |
| DISEApplicationEvents | Fires application events. |
| DISEApplicationWindowEvents | Provides access to the application window events. |
| DISEAssemblyChangeEvents | Assembly change events. |
| DISEAssemblyFamilyEvents | |
| DISEAssemblyRecomputeEvents | Represents a collection of assembly recompute events. |
| DISECommand | Provides interfaces for Visual Basic users to capture user input to process Solid Edge events. |
| DISECommandBarButtonEvents | A collection of CommandBarButtonEvent objects. |
| DISECommandEvents | |
| DISECommandWindowEvents | |
| DISEDocumentEvents | Fires document events. |
| DISEFileUIEvents | Fires file user interface events. |
| DISEhDCDisplayEvents | Fires display events. |
| DISEMouse | Provides interfaces for Visual Basic users to capture user input to process Solid Edge mouse events. |
| DISEMouseEvents | |
| DISEViewEvents | Fires view events. |
| DisplayEvents | Fires display events. |
| DividePartEvents | Represents a collection of DividedPart-based events. |
| DocumentEvents | Fires document events. |
| Documents | A collection of Document objects. |
| DraftBendTableEvents | Contains the AfterUpdate event. |
| DrawingViewEvents | Represents a collection of DrawingView events. |
| Environment | The menus and accelerators to a Window object. Defines the set of commands that can be run while a window associated to an environment is active. |
| Environments | A collection of Environment objects. |
| FaceStyle | An object in the FaceStyles collection. |
| FaceStyles | A collection of FaceStyle objects. |
| FamilyOfPartsEvents | Represents a collection of Family of Parts events. |
| FamilyOfPartsExEvents | |
| FeatureLibraryEvents | Represents a collection of Feature Library-based events. |
| FileUIEvents | Fires file user interface events. |
| FillStyle | Defines the fill characteristics of an enclosed object. |
| FillStyles | A collection of FillStyle objects. |
| GLDisplayEvents | Represents a collection of GLDisplay events. |
| HatchPatternStyle | A vector pattern that is used to fill a closed boundary. |
| HatchPatternStyles | A collection of HatchPatternStyle objects. |
| HighlightSet | Represents an occurrence of a Highlight set in Assembly, Draft, Part, or Sheet Metal documents. |
| HighlightSets | A collection of HighLightSet objects. |
| Insight | Insight Automation Object |
| InterDocumentUpdate | This interface will house methods for reporting, loading and saving the documents shown in the Component Tracker. |
| InterpartLink | |
| InterpartLinks | |
| ISEAccelerator | Represents a collection of KeyBinding objects. |
| ISEAccelerators | Represents a collection of Accelerator objects. |
| ISEAddIn | A control that represents a command added to Solid Edge through the AddIn interface. |
| ISEAddInEdgeBarEvents | |
| ISEAddInEdgeBarEventsEx | |
| ISEAddInEvents | A collection of AddInEvent objects. |
| ISEAddInEventsEx | A collection of AddInEvent objects. |
| ISEAddInEx | A control that represents a command added to Solid Edge through the AddIn interface. |
| ISEAddInEx2 | A control that represents a command added to Solid Edge through the AddIn interface. |
| ISEAddIns | A collection of AddIn objects. |
| ISEApplicationEvents | Fires application events. |
| ISEApplicationV8AfterDocumentOpenEvent | Fires document open event |
| ISEApplicationWindowEvents | Provides access to the application window events. |
| ISEAssemblyChangeEvents | Assembly change events. |
| ISEAssemblyFamilyEvents | |
| ISEAssemblyRecomputeEvents | Represents a collection of assembly recompute events. |
| ISEBlockTableEvents | Contains the AfterUpdate event. |
| ISECommand | Provides interfaces for Visual Basic users to capture user input to process Solid Edge events. |
| ISECommandBar | Represents all menus, toolbars, and pop-up menus in Solid Edge. |
| ISECommandBarButton | Represents buttons on toolbars and menus. |
| ISECommandBarButtonEvents | A collection of CommandBarButtonEvent objects. |
| ISECommandBarControl | Contains the properties and methods that are applicable to both CommandBarButton and CommandBarPopup objects. |
| ISECommandBarControls | Contains all of the buttons and pop-ups on a specific command bar. |
| ISECommandBarPopup | Represents pop-ups on toolbars and menus. |
| ISECommandBars | A collection of all of the command bars within a specific environment. |
| ISECommandCategories | A collection of command categories |
| ISECommandCategory | |
| ISECommandEvents | |
| ISECommandEx | Provides interfaces for Visual Basic users to capture user input to process Solid Edge events. |
| ISECommandInfo | |
| ISECommandWindowEvents | |
| ISEConnectorTableEvents | Contains the AfterUpdate event. |
| ISEDividePartEvents | Represents a collection of DividedPart-based events. |
| ISEDocumentEvents | Fires document events. |
| ISEDraftBendTableEvents | Contains the AfterUpdate event. |
| ISEDrawingViewEvents | Represents a collection of DrawingView events. |
| ISEDynamicEditEvents | Fires dynamic edit events. |
| ISEECEvents | SEEC Events |
| ISEFamilyOfPartsEvents | Represents a collection of Family of Parts events. |
| ISEFamilyOfPartsExEvents | |
| ISEFeatureLibraryEvents | Represents a collection of Feature Library-based events. |
| ISEFileUIEvents | Fires file user interface events. |
| ISEhDCDisplayEvents | Fires display events. |
| ISEIGLDisplayEvents | Represents a collection of GLDisplay events. |
| ISEKeyBinding | Provides information about an existing key binding. |
| ISELocateFilterEvents | |
| ISEModelRecomputeEvents | Fires model recompute events. |
| ISEMouse | Provides interfaces for Visual Basic users to capture user input to process Solid Edge mouse events. |
| ISEMouseEvents | |
| ISEMouseEx | |
| ISENewFileUIEvents | |
| ISEPartsListEvents | Contains the AfterUpdate event. |
| ISERenderEvents | Represents a collection of rendering events. |
| ISEShortCutMenuEvents | Event set for short-cut menu manipulations |
| ISEViewEvents | Fires view events. |
| ISolidEdgeAddIn | Provides an interface for add-ins to implement for Solid Edge to connect to them. |
| ISolidEdgeBar | |
| ISolidEdgeBarEx | |
| ISolidEdgeBarEx2 | |
| ISolidEdgeCommandBar | |
| ISolidEdgeRibbonBar | |
| ISolidEdgeRibbonBarEx | |
| KeyBinding | Provides information about an existing key binding. |
| Layer | An object in the Layers collection object. |
| Layers | A collection of Layer objects. |
| LinearStyle | Consists of the information required to represent a line graphically. |
| LinearStyles | A collection of LinearStyle objects. |
| MatTable | |
| ModelRecomputeEvents | Fires model recompute events. |
| Mouse | Provides interfaces for Visual Basic users to capture user input to process Solid Edge mouse events. |
| NewFileUIEvents | |
| PartsListEvents | Contains the AfterUpdate event. |
| Properties | A collection of Property objects. |
| Property | A user-defined document attribute. |
| PropertySets | A collection of PropertySet objects. |
| QueryObjects | Represents the collection of objects returned by a query. |
| RadialMenu | |
| Reference | Represents an object that references another object (a part or assembly, for example). |
| RenderEvents | Represents a collection of rendering events. |
| RibbonBar | |
| RibbonBarControl | |
| RibbonBarControls | |
| RibbonBarGroup | |
| RibbonBarGroups | |
| RibbonBars | |
| RibbonBarTab | |
| RibbonBarTabs | |
| RibbonBarTheme | |
| RibbonBarThemes | |
| RoutingSlip | Distributes a document to recipients either at one time or sequentially. |
| SectionView | Automation object for a section view in a Part or Assembly document. |
| SectionViews | Collection of section views. |
| SEECEvents | SEEC Events |
| SEGenericCollection | Represents a collection of AttachedProperty objects. |
| SelectSet | A temporary grouping of one or more selected objects. |
| Sensor | Represents an occurrence of a Sensor feature in an Assembly document, a Part document, or a Sheet Metal document. |
| Sensors | A collection of Sensor objects. |
| SheetMetalSensors | Represents a collection of sensors on a SheetMetalDocument. |
| ShortcutMenuEvents | |
| SolidEdgeDocument | |
| SolidEdgeInsightXT | InsightXT Automation Object. |
| SolidEdgeTCE | Solid Edge Teamcenter Automation object. |
| SummaryInfo | Contains information about a document. |
| SwitchWindowCust | |
| Symbol2d | Allows you to review or manipulate the symbol geometry, the attachment between a symbol and a source document, and the user property. |
| SymbolProperties | A collection of SymbolProperty objects. |
| Symbols | A collection of Symbol objects. |
| TextCharStyle | Contains a set of character characteristics that can be applied as a set to the active text. |
| TextCharStyles | A collection of TextCharStyle objects. |
| TextStyle | Contains characteristics to apply to the active paragraph. |
| TextStyles | A collection of TextStyle objects. |
| UnitOfMeasure | The UnitOfMeasure object allows you to set and return the unit type and precision for each category, depending on the index of the unit. |
| UnitsOfMeasure | Allows you to convert internal measurement units to user-specified measurement units. |
| variable | Associates a name with a numeric value. |
| VariableList | A list of Variable objects returned from a query. |
| Variables | A collection of Variable objects. |
| View | Provides methods and properties that allow you to manipulate Solid Edge window views. |
| ViewEvents | Fires view events. |
| ViewStyle | Contains a collection of properties that control view rendering. |
| ViewStyles | A collection of ViewStyle objects. |
| Window | Provides support for adjusting the size of the actual viewing area. |
| Windows | A collection of Window objects. |