Solid Edge Geometry Type Library
IsRational Property
Description
Returns True if the referenced object is rational.
Property type
Read-only property
Syntax
Visual Basic
Public Property IsRational As Boolean
Remarks
Rational (that is, a weight is assigned to every pole).
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objBody As SolidEdgeGeometry.Body
    Dim objEdges As Object
    Dim objBSplnEdge As SolidEdgeGeometry.Edge
    Dim objBSpln As SolidEdgeGeometry.BSplineCurve
    Const TESTFILE = "T:\vbtests\testcases\Curve3d.par"
    Dim bRational As Boolean
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    ' Open the TestFile
    Set objDoc = objApp.Documents.Open(TESTFILE)
    ' Get the Model object
    Set objBody = objDoc.Models(1).Body
    ' Get Edges Collection object
    Set objEdges = objBody.Edges(EdgeType:=igQuerySpline)
    ' Get a Spline Edge
    Set objBSplnEdge = objEdges(1)
    ' Get the BSpline Curve
    Set objBSpln = objBSplnEdge.Geometry
    ' Get the Rational property
    bRational = objBSpln.IsRational
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objBody = Nothing
    Set objBSplnEdge = Nothing
    Set objEdges = Nothing
    Set objBSpln = Nothing
End Sub
See Also

BSplineCurve Object  | BSplineCurve Members