Solid Edge Geometry Type Library
GetNumKnots Method
Returns the number of knots for the referenced object.
Description
Returns the number of knots in the referenced object.
Syntax
Visual Basic
Public Sub GetNumKnots( _
   ByRef NumKnots() As Long _
) 
Parameters
NumKnots
Returns the number of knots for the referenced object.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objBody As SolidEdgeGeometry.Body
    Dim objFaces As Object
    Dim objBSplnSrf As SolidEdgeGeometry.BSplineSurface
    Const TESTFILE = "T:\vbtests\testcases\Curve3d.par"
    Dim lngKnots() As Long
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    ' Open the TestFile
    Set objDoc = objApp.Documents.Open(TESTFILE)
    ' Get the Model object
    Set objBody = objDoc.Models(1).Body
    ' Get the Faces Collection object
    Set objFaces = objBody.Faces(FaceType:=igQuerySpline)
    ' Get a BSpline Surace
    Set objBSplnSrf = objFaces(1).Geometry
    ' Get the KnotCount of BSpline Surface
    Call objBSplnSrf.GetNumKnots(lngKnots())
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objBody = Nothing
    Set objFaces = Nothing
    Set objBSplnSrf = Nothing
End Sub
See Also

BSplineSurface Object  | BSplineSurface Members