Solid Edge Geometry Type Library
GetOrder Method
Returns the order in the u and v directions, respectively, for BSplineSurface object and the order of the B-Spline for BSplineCurve and ParamBSpline objects.
Description
Returns the order for the referenced object.
Syntax
Visual Basic
Public Sub GetOrder( _
   ByRef Order() As Long _
) 
Parameters
Order
Returns the order in the u and v directions, respectively, for BSplineSurface object and the order of the B-Spline for BSplineCurve and ParamBSpline objects.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objBody As SolidEdgeGeometry.Body
    Dim objFaces As Object
    Dim objBSplnSrf As SolidEdgeGeometry.BSplineSurface
    Const TESTFILE = "T:\vbtests\testcases\Curve3d.par"
    Dim lngOrder() As Long
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    ' Open the TestFile
    Set objDoc = objApp.Documents.Open(TESTFILE)
    ' Get the Model object
    Set objBody = objDoc.Models(1).Body
    ' Get the Faces Collection object
    Set objFaces = objBody.Faces(FaceType:=igQuerySpline)
    ' Get a BSpline Surace
    Set objBSplnSrf = objFaces(1).Geometry
    ' Get the Order of BSpline Surface
    Call objBSplnSrf.GetOrder(lngOrder())
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objBody = Nothing
    Set objFaces = Nothing
    Set objBSplnSrf = Nothing
End Sub
See Also

BSplineSurface Object  | BSplineSurface Members