Solid Edge Geometry Type Library
Shells Property
Description
Returns a Shells collection object.
Property type
Read-only property
Syntax
Visual Basic
Public Property Shells As Object
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFrameWork.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objBody As SolidEdgeGeometry.Body
    Dim objBShells As SolidEdgeGeometry.Shells
    Const TESTFILE = "T:\vbtests\testcases\freeform.par"
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    Call objDoc.Close
    ' opening the test case file
    Set objDoc = objApp.Documents.Open(TESTFILE)
    ' getting the body object of the model
    Set objBody = objDoc.Models(1).Body
    ' getting the Shells object for the body
    Set objBShells = objBody.Shells
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objBody = Nothing
    Set objBShells = Nothing
End Sub
See Also

Body Object  | Body Members